简体中文  | English  | Español  | 日本語  | Português
Skip Navigation Links
Home
Products
Library
Company
Contact Us
Site Map
What's New at
ATI Industrial Automation
 
 
 

ATI to introduce new QC-1210 Robotic Tool Changer at IMTS 2008

New Tool Changer developed for robots that can handle up to 1200 kg loads

Apex, NC,  August 28, 2008
 

On September 8-13 at the 2008 International Manufacturing Technology show in Chicago, IL, ATI Industrial Automation will introduce the new QC-1210 Heavy Automation Robotic Tool Changer. The QC-1210 was developed for robots that can handle up to 1200 kg loads and features three of ATI's patented Fail-Safe locking mechanisms.  The new Tool Changer can mount up to six utility modules using a common mounting pattern. Also on display will be, ATI's new Net F/T Force/Torque Sensor System. The Net F/T System measures six components of force and torque (Fx, Fy, Fz, Tx, Ty, Tz) and provides an EtherNet/IP™ and CAN bus communication interface, and is compatible with standard Ethernet. At Booth # B-6416, ATI will also have all of their newest end-effector products on display, including Robotic Tool Changers, Multi-axis Force/Torque Sensors, Robotic Deburring and Finishing Tools, Robotic Collision Sensors, Rotary Joints, and Compliance Devices.

ATI_QC-1210_Tool_Changer.jpg

Many other exhibitors at IMTS will be featuring ATI products. Visit these companies to see ATI products in action:

Acme Manufacturing Co. - Booth # B-7241

Fanuc Robotics - Booth # A-8418

Hirschman Automation - Booth # D-4100

Makino - Booth # D-4101, A-8301

Mazak - Booth # A-8101

Motoman - Booth # B-6400

Okuma/Fanuc - Booth # A-8200, A-8745

Weldon Solutions - Booth # B-7410

Contact us at 919-772-0115 if you would like a free pass to the show and be sure to stop by our booth (# B-6416).

More information on IMTS here.

More information on our QC-1210 Heavy Automation Tool Changer here.

More information on our Robotic Tool Changers here.